12/30/2010 12:01 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, You need to put in hardware configuration the same CPU like real one. In your case 315-2PN/DP firmware 3.2. You can chose it from Hardware Configuration in Profile "Standard". Look at attachment. Merry Christmas! Best regards, Hristo Mihalev |
1/7/2011 9:43 AM | |
Joined: 12/8/2010 Last visit: 9/16/2020 Posts: 10 Rating: (0) |
Hi Hosseini, I have version 5.4 and SP4 does it work ? and inspite of the fact that I updated my elekctronic catalog I could not have CPU ver 3.2 I can only have CPU ver 3.1 |
1/7/2011 9:58 AM | |
Joined: 12/8/2010 Last visit: 9/16/2020 Posts: 10 Rating: (0) |
Hi Umencho, my config as in attached file, I wonder does it create problem later on. |
1/7/2011 2:46 PM | |||||
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Configuration with older software versions: If the new functions are not required, you can configure the module in STEP 7 as predecessor (FW V3.1) with the latter's scope of functions.
Best regards, Hristo Mihalev |
||||
1/7/2011 4:29 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Dear Volkan I have STEP7 5.5 with latest update of hardware downloaded from here.Check the attachment for list the V3.2 of CPU you want. STEP 7 Hardware Support Packages (HSPs - as at 12/2010) for installing hardware updates in the Hardware Configuration |
This contribution was helpful to1 thankful Users |