7/6/2017 11:05 AM | |
Posts: 14 Rating: (1) |
Hi everyone, I have a simple USB - barcode scanner TaoTronics BS014 connected to my IOT2040. The device seems to be detected properly by the IOT2040. The scanner simulates a keyboard.
In debian-like systems, there was a /dev/ttyUSB, where I simply could log the data from an USB-device. In my yocto - image (which is nearly the same as the meta-iot-example), there is no ttyUSB. So my question is, if there is another way to get the data from the barcode scanner? Here some addional and maybe helpful informations:
ID 13ba:0018 should be the barcode scanner:
I am grateful for any suggestions. Greetings PalinPalin |
This contribution was helpful to1 thankful Users |
12/6/2017 11:35 PM | |
Posts: 37 Rating: (3) |
Hi, see also this thread for some information how to use a barcode scanner together with IoT2000, especially with Node-Red: https://support.industry.siemens.com/tf/ww/en/posts/usb-node-red/179852/?page=0&pageSize=10 Michael |
Last edited by: turner42 at: 12/7/2017 12:07:52 AM |
|