2/13/2020 5:37 PM | |
Joined: 6/19/2008 Last visit: 6/1/2023 Posts: 46 Rating: (4) |
Thx a lot guys :D But this brings more questions ;) 1. So there is no specific addresing like A 4.0 but somehow whole DO module will by assigned to one Byte ? How do I know which Byte is dedicated to which Module ? Is like: Module in slot 0 - Byte 0 2. Do I think right (I have 8 DO at module) that in assigned Byte for example Bit 0 will be DO channel 0 (ie. Q x.0) and Bit 1 will be DO channel 1 (ie. Q x.1) etc ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/14/2020 06:12:32New subject after splitting |
|
2/13/2020 5:42 PM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33051 Rating: (4082) |
By S5 there is no hardware configuration like S7. Can you make photo of the S5 with modules? Is it a S5-95U? |
2/13/2020 6:01 PM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33051 Rating: (4082) |
If it is a S5-95U, then take a look at attachment. The complete manual can you download here: AttachmentPages.zip (306 Downloads) |