10/12/2012 2:57 PM | |
Posts: 9 Rating: (3) |
Dear Sir Thank you for your information. Warm Regards Krishna...
|
10/13/2012 12:10 PM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Dear experts, I am also faced the same problem. Not only the retentive range, none of the CPU property will upload while doing upload operation. ( retentive property, cpu clock, I/O modules will upload with default address(not with configured address) etc.) After that I have send support request. Then i got the reply like this. During upload STEP 7 uploads the hardware configuration from the CPU, including any modules (SM, SB, or CM). Please refer the same in the section 11.14 of manual :-http://support.automation.siemens.com/WW/view/en/39710145 But still the problem is not rectified. One more thing, why should we copy paste the blocks?? Just click on newly created project's PROGRAM BLOCK option, then we can see the upload shortcut will be enabled. so that we can directly upload the blocks. (I think with tia v 10.5 that option is not available) Regards
|
Last edited by: vipz at: 10/13/2012 4:22 PM
|
|
This contribution was helpful to1 thankful Users |
10/15/2012 1:01 PM | |
Joined: 8/31/2010 Last visit: 5/15/2024 Posts: 1510 Rating: (222) |
Steps to upload the configuration of a S7-1200 using STEP 7 V11 SP2- Watch it Online!! |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
10/17/2012 8:20 AM | |
Posts: 25 Rating: (0) |
Very true.That's why I hope it wil be fixed soon... |
Follow us on