1/12/2011 12:56 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Take a look there - How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs? Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
5/15/2011 7:18 PM | |
Posts: 167 Rating:
|
there are two system file on the SIEMENS MMCs that when you format them this two file will erased and after that you can not use MMC on the CPUs and also as i know reviving The MMC is hard and almost impossible.that is why UMENCHO has said you can use it just in camera not CPUs. |
5/18/2011 8:15 AM | |
Posts: 24 Rating:
|
Just curious, is there really no way to revive Siemens mmc? It'll be good if someone can share, just in case! |
5/18/2011 8:22 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
So, there exist a lot ways for everything. Let's assume here anybody doesn't want to share the ways. Thread is closed. Best regards, Hristo Mihalev |
5/21/2011 10:35 AM | |
Joined: 5/28/2008 Last visit: 7/17/2024 Posts: 4511 Rating:
|
Hello, Resst MMC means: Delete all user data. Fromat MMC means: Delete every thing on the MMC which includes the user data and also system files. So what is the rason that make any user format the MMC? As Umencho's tells that there are always ways to do any thing. But why we go for format the MMC and then try find a way how to restore the system files?!! |
Ayman Elotaify |
|
5/21/2011 10:48 AM | |
Posts: 8946 Rating:
|
If you like to use standard MMC as SIMATIC - MMC, it will not be possible, as far as I know. Also, the SIMATIC MMC use different memory control to give them a longer live. So, even if the price is higher, you should use the original Siemens - equipment and you must not format one of this MMC! There are also a lot of other threads concerning this topic, just use the search - function. |
Last edited by: IBN-Service at: 5/21/2011 10:48 AM |
|
Follow us on