4/28/2022 3:00 PM | |
Joined: 4/19/2022 Last visit: 11/4/2022 Posts: 3 Rating: (0) |
You will first need to navigate and open the Graphic that contains the point we will be modifying. Once you are on the correct Graphic you will then need to place it in Edit/Engineering Mode as long as you have the access rights. Then you will click on the point you want to edit, make sure that you have the Symbol Instance Properties View open. In the Symbol Instance Properties popup you will need to scroll down until you find the Command and Navigate dropdown. In this dropdown you will see the Target box. Make sure that this is empty so that it will no longer bring you to another graphic when it is double clicked. You can also change the number of clicks it takes to open in the Trigger area.
AttachmentTrigger Point.pdf (495 Downloads) |
4/29/2022 9:56 AM | |
Joined: 3/23/2022 Last visit: 5/10/2022 Posts: 12 Rating: (0) |
Thank Bombo107. I tried as you said but it doesn't work. |
5/9/2022 8:25 AM | |
Joined: 4/28/2015 Last visit: 8/12/2024 Posts: 84 Rating: (42) |
Hi THE DANG, Today I was able to talk to one of my colleagues from the HQ support team and he confirmed that it is not possible to disable the double click navigation behavior. |
Follow us on