3/7/2020 2:25 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33157 Rating: (4095)
|
Are limit switches for out and in on the cylinders? |
3/7/2020 3:59 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33157 Rating: (4095)
|
Do you like this solution? But note: AttachmentTwo-hand_and_two_cylinder_0BA8.Standard.zip (346 Downloads) |
3/8/2020 10:22 AM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33157 Rating: (4095)
|
Try this.
AttachmentTwo-hand_and_two_cylinder_0BA8.Standard_V2.zip (303 Downloads) |
3/11/2020 1:56 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33157 Rating: (4095)
|
In attachment a video of the simulation. Which LOGO! have you exactly? Please write the exact order number und the firmware version. Which LSC Version have you? AttachmentSimulation.zip (286 Downloads) |
3/13/2020 10:38 PM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33157 Rating: (4095)
|
Have you tried the second solution? |
3/14/2020 8:26 AM | |
Posts: 19 Rating: (1) |
Hello, On the specification I see Logo! 8.FS4 and in another Logo! 0.BA7 Hope I answer to your request. |
3/20/2020 2:26 PM | |
Posts: 19 Rating: (1) |
Hello, did this reference is fine for you please? Logo!Softcomfort(2016-07-14 16-34 |
3/20/2020 2:55 PM | |
Posts: 19 Rating: (1) |
Please, where I have to look or search the reference you want? |
3/20/2020 3:25 PM | |
Posts: 19 Rating: (1) |
I will send you very soon the ref as you shown me. Thank you for the clear explanation. I have another question: I can't open your program Twohand1.lsc??? |
3/20/2020 4:24 PM | |
Posts: 19 Rating: (1) |
This time I had. Hope that this will solve my problem!!! |
3/20/2020 4:51 PM | |
Posts: 19 Rating: (1) |
Hello, I recap the principle of runing of cylinders. Please, se the document in appendix. I1 is the signal which is on when both hand are pushing the button, so comparing to before, now I have only one signal for both hand. Please, I have two demand now: 1) to adapt the previous program that I use I1 for both hands, and I6 for start blowing. 2) to explain me why or how to load on logo! because your previous program I didn't been able to load on logo! Thank you in advance. AttachmentPrinciple of programe.pdf (197 Downloads) |
3/20/2020 10:43 PM | |
Posts: 19 Rating: (1) |
Hello, yes , you are right. thank you |
3/20/2020 10:48 PM | |
Posts: 19 Rating: (1) |
Hello, to 1), the I6 switch the output Q2 to start blowing air. to 2), I saw during manipulation that shown also the FS4. thank you 😊 |
3/22/2020 6:04 AM | |
Joined: 12/18/2014 Last visit: 6/6/2024 Posts: 33157 Rating: (4095)
|
I hope now it is so as you want....
AttachmentTwo_cylinders_FS4.zip (196 Downloads) |
This contribution was helpful to1 thankful Users |
3/22/2020 6:50 PM | |
Joined: 12/30/2018 Last visit: 5/10/2024 Posts: 3 Rating: (0) |
krijg fout melding bij open van laatste programma van 22-03-2020 |
Follow us on