12/13/2017 5:41 PM | |
Joined: 10/8/2015 Last visit: 5/21/2024 Posts: 14 Rating: (0) |
Hi all, I'm using Simotion Scout v4.5, now I want integrate Wincc flex 2008 sp3 with it. I find the manual on internet & follow it. Link manual as below https://support.industry.siemens.com/cs/ww/en/view/91197964 But after I installed Wincc flex & install package integration with Simotion. I cannot file the tab " Insert HMI" follow instruction (attachment image) & also cannot file my HMI project in Simotion Scout I can open a Simotion project already have integration of HMI project (attachment image) without error "missing package" but just only the HMI project not show follow manual I tried to uninstall Wincc flex & installed it again (include package integration of Simotion also) but the Insert HMI tab still not appear. Anybody can help me for this problem? |
Last edited by: Jen_Moderator at: 12/14/2017 9:50:31 AMInserted right link. |
|
12/14/2017 9:46 AM | |
Joined: 10/11/2006 Last visit: 6/5/2024 Posts: 5857 Rating: (793)
|
Hi, for integration WinCC flex in Scout, please find information stepbyStep in some screens in attached PDF AttachmentHMI integration.pdf (124 Downloads) |
With best regards, |
|
12/14/2017 7:06 PM | |
Joined: 10/8/2015 Last visit: 5/21/2024 Posts: 14 Rating: (0) |
Thank all, My problem already solved ! |