1/23/2011 8:41 AM | |
Posts: 20 Rating:
|
Hi dear users, I have a problem in my profibus,I have added a new station with ET200U to my profibus,but it dosen't work and I have bus fault on my IM308. I have attached my configuration that configured by COM PROFIBUS V 5.1 I need your help thanks alot Attachmentlast.zip (84 Downloads) |
1/24/2011 8:03 AM | |
Joined: 10/7/2005 Last visit: 6/24/2024 Posts: 3008 Rating:
|
Hello Marcopolo I can't find anything obvious wrong in your COMPB config and suggest you check/try the following: 1.) What is the part number of your IM318? A 6ES5 318-8MB11 can NOT be used anymore and you'll need either an -8MB12or -8MB13(see also HERE for more) 2.) Cabling and Plug (perhaps a bad connection in the plug, can you try to swap Plugs around with a working DP Slave?). 3.) Is the physical configuration of your ET200U the same as your COMPB config (e.g. check your IM part number andmake sure it is in fact a 6ES5 318-8MB1x, check thatyou have onlyone 8DI followed byone 8DQ card in it). 4.) What CPU is in your S5 anddo you perhaps a DB1 with an I/O list in it?If so, you'll need to add the new I/O addresses to it and Cold restart your CPU (see the CPUmanual for more on this). 5.) You used Adress 0 for the Input and Output Byte, verify that this is NOT used elsewhere in the central or any expansion racks rack and/or try a different free address range for your DI and DQ card. That's all I can think of for now, I hope this helps and please let us know what you find. |
Cheers |
|
1/29/2011 9:04 AM | |
Posts: 20 Rating:
|
Dear Ayman Thanks,but resistance also is ok !!!! |
2/3/2011 1:27 PM | |
Joined: 5/26/2007 Last visit: 6/24/2024 Posts: 127 Rating:
|
how far is this et200? check the overall distance is supported by the profibus speed that you use. |
2/6/2011 12:00 PM | |
Posts: 20 Rating:
|
Dear Sulung Thanks for your comment,I have added to my line only 20 mt. Also I have changed my baudrate, but ... it didn't work. |
2/6/2011 12:06 PM | |
Posts: 20 Rating:
|
Dear Late My profibus connector is the new one and I have observed in/out cable. I haver attached my IM lable and also dip switch. Thanks for your last comment. AttachmentPIC.zip (76 Downloads) |
Follow us on