6/5/2015 9:30 AM | |
Joined: 5/20/2015 Last visit: 4/29/2024 Posts: 216 Rating: (3) |
hellow wizard, i am working on programming with fm350-2 with cpu 315 2dp, Now thing is that i want to use all the eight channels as pulse and direction mode, unfortunatly in the sample program library 'fm_cntli' using FC2_CNT2_CTR they have give UDT1 with just four channel words ie. CHECKBACK_SIGNALS.USER_STAT_WORD0 - -to CHECKBACK_SIGNALS.USER_STAT_WORD3 when i modify UDT1 upto CHECKBACK_SIGNALS.USER_STAT_WORD7 nothing is Working. please help boss. ------------ |
Last edited by: gabbar at: 6/5/2015 9:32:32 AMLast edited by: gabbar at: 6/5/2015 11:18:57 AMLast edited by: CS Moderator at: 6/7/2015 8:50:19 AMsplitting Let's do it... |
|
6/5/2015 10:40 AM | |
Joined: 4/24/2006 Last visit: 5/23/2024 Posts: 8657 Rating: (1154) |
Hello Gabbar, Here is a link to manual: SIMATIC S7-300 FM 350-2 Counter Module See page 51. Here you can define which values you want to read through direct access. And these values are in DB in the range: Checkback_signals_user_stat_word 0 to 3 Best regards, Wizard |
6/5/2015 11:18 AM | |
Joined: 5/20/2015 Last visit: 4/29/2024 Posts: 216 Rating: (3) |
|
Let's do it... |
|
6/5/2015 11:28 AM | |
Joined: 5/20/2015 Last visit: 4/29/2024 Posts: 216 Rating: (3) |
|
Let's do it... |
|
6/5/2015 1:51 PM | |
Joined: 4/24/2006 Last visit: 5/23/2024 Posts: 8657 Rating: (1154) |
Hello, When you use FB4 "CNT2RDPN", you need to generate the DB. Best regards, Wizard
|
6/8/2015 8:09 AM | |
Joined: 4/24/2006 Last visit: 5/23/2024 Posts: 8657 Rating: (1154) |
Hello Gabbar, Perhaps you could post your project. Best regards, Wizard |