1/26/2015 3:14 AM | |
Posts: 28 Rating: (0) |
Dear sir I orders one of card CP 527 PLC s5 with code 6AV1242-0AB10 to replace the card CP 257 at the factory with the same code. when I intallls at the site,I dowload progame to CP(use software COM GRAPH) and set on the CP 527 for either for high or slow monitor resolution,the led on CP show green(attach file) but the CP 527 can't not connect to monitor,the monitor show :no signal immediately. when i intalls the old card CP527 of factory.its ok coud you help me to sovle issues. Attachmentanh.zip (270 Downloads) |
Last edited by: nguyenlong89hui at: 1/26/2015 2:05 PM |
|
1/26/2015 4:13 PM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating: (90) |
Hello nguyenlong89hui Did you checked the jumper settings on the new card.The SSNr and communication marker range should be set by using jumpers. Did you placed the RGB connectors in the same sequence? A CP527 card uses sync on green signal. If you connect the wrong lead to the G connector, you might get no image on the monitor. Kind regards, BV |
1/29/2015 2:40 AM | |
Posts: 28 Rating: (0) |
this is a picture of working CP527's board sir, when connected to the screen, we need 4-wire(R,G,B,S) or 3-wire ? |
2/1/2015 2:09 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
|
My Forum is the place to personalize your profile, |
|