9/25/2014 9:28 AM | |
Posts: 515 Rating: (56) |
Dear Experts, in one of my previous posts H-H provided me with this part number6ES7 322-8BH10-0AB0as requested. But in the technical spec of the same the current rating mentioned is 0.5A where i need more than that to drive some devices along with the channel diagnostics. also i found this fail safe module6ES7326-2BF10-0AB0with 2A current rating. is it possible to use this module with the CPU central configuration (CPU used is 315-2 PN/DP) for the requirement. is this module permitted to use along with a standard CPU and other standard I/O's. And should i need to consider the fail safe software for the mentioned module for the diagnostics? Could anyone help me out please
|