2/13/2011 1:50 AM | |
Joined: 10/7/2005 Last visit: 7/30/2024 Posts: 3013 Rating:
|
Hello JohnS57 while I can't help you with the schematics of your machine (best place to ask is the manufacturer of the machine should he still exist), I can at least point to https://support.automation.siemens.comwhere you can search for (and hopefully find)the manuals for your S5 gear (CPU, OP's etc.). These will at least give you for example the information about the CPU's LED status, CPU start up behaviour, how to diagnose it etc. etc. for the Siemens relevant parts of your system. I hope this helps, pelase let us know what you find out and should you have more question come back here to ask (and please provide us with the Siemens relevant part numbers, CPU type, ISTACK infoetc.. The more details you can give us about your control system and problem, the better). |
Cheers |
|
2/15/2011 12:31 AM | |
Joined: 10/7/2005 Last visit: 7/30/2024 Posts: 3013 Rating:
|
Hello JohnS57 whiel your part number is not complete (the last few digits are missing), there are at least afew manuals available for the the IP252 and IP244 at the link below: http://support.automation.siemens.com/WW/view/en/10805137/133300 I hope this helps |
Cheers |
|
2/15/2011 9:55 AM | |
Posts: 376 Rating:
|
Hello JohnS57, I think you use the CPU943 with the order number 6ES5 943-7UB11. The manual SIMATIC S5, S5-115U, Programmable Controller for following CPU types finds you here: http://support.automation.siemens.com/WW/view/en/1085937 CPU types: CPU 941-7UB11CPU 942-7UB11CPU 943-7UB11 and CPU 943-7UB21CPU 944-7UB11 and CPU 944-7UB21 As an attachment I send you the following manual as pdf-file. S5-115U_OperationList_6ES5997-7LA21.pdf Operations List for the CPU 941/942/943 and 944. Question. Do you have the complete order number for your hardware IP252 and IP242? Do you have new information about your problem? Best regards Gucci AttachmentS5-115U_OperationList_6ES5997-7LA21.pdf (195 Downloads) |
2/17/2011 2:22 AM | |
Posts: 6 Rating:
|
So far here is what I think what happened. They had it running (booted)and the AC voltage was too high. Something that uses ACmaybeheat or AC related got burned out. The system was still measuring the heat that nigh or was past the post test of the program, but would of not been able to run a cycle if they had tried. Since they never got that far, it seemed to them it was working. In the AM after things cooled down, the boot of the systemwas now seeing therewas a hazard condition and goes in to programmed fault.If I had a schematic of the Van Dorn wiring I could track down what items connect to the AC outside of the controller's power supply. An example could be the terminal couple(s). Many use a configuration with a Wheatstone bridgewhere a external voltage is applied.(see http://www.sensorland.com/HowPage017.html mid page for more info). It is also possible that the system looks at the voltage drop on heating elements and motor windings as a pre test to the boot cycle. The other that can happen are items that are measuring devices see thevalue measuredas mid range. It therewas an open, the system see the rail voltage (to one extreme) so itperceives an unacceptable measurement.Based on the observation I have already made, thisline maybe worth further investigation and explains why it booted the night before.
Does anyone have any ideas I could pass on to him? Thanks, john |
Follow us on