7/11/2022 5:30 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
hello, for that you need a MMC Card Reader (buitlin in FiledPG or USB Prommer 6ES7792-0AA00-0XA0 ) A normal Card Reader can read this type of Cards. |
7/11/2022 8:15 AM | |
Joined: 7/9/2015 Last visit: 5/17/2024 Posts: 3833 Rating: (557)
|
Hi, please also check this FAQ: How do you load projects on a memory card and back to a PG/PC?Regards, Towome |
|
|
7/11/2022 10:57 AM | |
Joined: 1/17/2013 Last visit: 5/16/2024 Posts: 1081 Rating: (6) |
Dear Unreality, How can I copy project code in MMC into my PG without source file (the project made from TIA V14) ? Best Regards, Vorapob |
Best Regards, |
|
7/11/2022 11:06 AM | |
Joined: 1/17/2013 Last visit: 5/16/2024 Posts: 1081 Rating: (6) |
Dear ChristophD, I have PG and I would like to know if I copy the data into MMC card to PG can I copy this data into new MMC card ? Is the machine can run in normal operation if I use new MMC card in old PLC. The machine use S7-317F with TIA V14 as I knew from the technician. Best Regards, Vorapob |
Best Regards, |
|
7/13/2022 6:21 AM | |
Joined: 1/17/2013 Last visit: 5/16/2024 Posts: 1081 Rating: (6) |
Dear ChristophD, I try to use MMC card with my PG in order to copy and backup project from PLC S7-317F but it has message "Restrictions for uploading to PG/PC ". How can I do in order to copy this project file ? Best Regards, Vorapob |
Best Regards, |
|
Follow us on