Industry Online Support
Technical Forum
2/22/2024 5:46 PM | |
Joined: 5/4/2023 Last visit: 6/3/2024 Posts: 2 Rating: (0) |
Hi, I'm using a UCP ( MTP1000) and I have this exact issue. I've configured the system as local user management, added a user (admin rights) in TIA and enabled edge computing / remote access on the panel. I can access the edge management, and the user access at the panel address (192.168.x.x) via browser on development machine. If the runtime isn't running I get a message telling me that the runtime isn't running. But if I start the runtime via the panel then I get OP's message about missing 'IdentityProviderURL' and asking me to 'fix UMC configuration' - but it's not UMC, it's locally managed - I should just be getting a user login request. I have satisfied all the requirements in the instructions in the attached image. I enabled encrypted connection and installed the certificate pack in to Trusted Root. But I still get a warning and the site is not HTTPS - I read somewhere that it should be HTTPS (maybe it won't allow sending login details over unencrypted connection?) Do you have any suggestions? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/23/2024 11:18:54New subject after splitting |
|
Follow us on