2/16/2024 6:59 PM | |
Joined: 6/13/2023 Last visit: 4/26/2024 Posts: 13 Rating: (0) |
Thank you, I'll post in the other conference then. |
2/23/2024 7:52 AM | |
Joined: 8/3/2009 Last visit: 5/27/2024 Posts: 12984 Rating: (1653)
|
Hello AutoGen_4505780 I did a few tests with Logo 8.3 and a Unified comfort panel using Modbus TCP and it seems to work... I did only a few basic tests if I could reach some address areas and so on.. (V und VM addressarea in Logo addressing with 0x1-0x16 and 4×400001 (Word and/or +-Int)) some information are also in https://support.industry.siemens.com/cs/ww/en/view/109811957 -> I did not used it in a project or on a productive machine but generally it seems to work But I think it is no official solution or I have not found any examples on Siemens Website EDIT: I added some additional information in this TOPIC: I hope it helps bye Murof |
Last edited by: Murof at: 03/14/2024 09:23:50If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on