11/2/2022 1:26 PM | |
Joined: 4/23/2010 Last visit: 5/17/2024 Posts: 9 Rating: (0) |
I wrestled with this for several hours and have come up with a work around that works well. It is based upon the script offered in the WinCC Unified Tips offered in this FAQ: https://support.industry.siemens.com/cs/pl/en/view/109810540 I used the "1.2 Access the instance of a pop-up via its title" case to accomplish this. It basically matches the pop-up name, and I used the ui.PopupScreenWindows(i).Close(); method to close the pop-up. I made it a global script so that I could just pass the pop-up name into script since I have several pop-up windows in my project. I have attached a picture of the code.
|
This contribution was helpful to2 thankful Users |
Follow us on