2/29/2024 8:53 AM | |
Joined: 1/21/2013 Last visit: 6/7/2024 Posts: 2861 Rating: (458)
|
Hi,
The system function "CreateScreenshot" is only available for WinCC Unified Comfort Panel. Since you are using an MTP1500, this is fine, but the panel is not a Windows device, so you need to specify the path in a Unix format. And of course, the path must be available and writable. To save locally on the device, you can use '/home/industrial' or '/home/scs/' if you are doing it in a scheduled task. To use an SD card, use '/media/simatic/X51', for a USB stick use '/media/simatic/X61', '/media/simatic/X62', '/media/simatic/X63' or '/media/simatic/X64', depending on the interface used. And when saving to a network share, you must use '/net/mount'. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on