3/12/2024 10:40 AM | |
Joined: 4/24/2006 Last visit: 5/2/2024 Posts: 8629 Rating: (1147) |
Hello, Perhaps the following link might help: Best regards, Wizard |
3/15/2024 10:47 AM | |
Joined: 8/3/2009 Last visit: 4/30/2024 Posts: 12869 Rating: (1643)
|
Hello Nkuthal Which TIA Portal Version do you use? It is important because the Basic Panels 1st Generation only have a V12 Image also in newer TIA Versions. The PLC Sim changed something since V14 and then older Panel Images cannot connect in simulation to PLC Sim: https://support.industry.siemens.com/cs/de/en/view/109742764 This means if you have TIA V14 or newer then you cannot connect a Basic Panel 1st Gen to your PLC Simulation (S71200/1500) (S7300/400 would work) But with real HW it will work Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/19/2024 5:59 AM | |
Joined: 10/12/2023 Last visit: 4/29/2024 Posts: 18 Rating: (1) |
Thanks I am using V18. |
No such thing as a stupid question |
|
Follow us on