5/25/2013 8:37 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi Raffy, You have a file GSD? GSD files - Expansion module PAC PROFIBUS DP, 7KM9300 ... |
Last edited by: Ste39 at: 5/25/2013 8:46 AM |
|
5/25/2013 9:08 AM | |
Posts: 209 Rating: (2) |
Hi ste39, Now I understand...so I need a GSD file for hardware add-ons....do you have a link on how to use this GSD files?? Thanks... |
5/25/2013 9:49 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi Raffy, The links above are the GSD file of the Sentron and here's how to do install them in the hardware catalog. How do you integrate a GSD file into the STEP 7 HW Config for ... Hope this help |
6/17/2013 8:07 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi Raffy, From your diagram looks good but as long as the LED is not green you can not communicate. If the LED is flashing orange means that: Color Status Description Measures Orange Flashing Hardware fault on the expansion module or the SENTRON PAC power meter, e.g.: • 12 V too weak or not present • SRAM fault • Flash fault • EEPROM faultReplace the PAC PROFIBUS DP expansion module and/or the SENTRON PAC power meter. |
Last edited by: Ste39 at: 6/17/2013 11:25 AM |
|
Follow us on