9/11/2013 11:36 AM | |
Joined: 5/12/2006 Last visit: 11/18/2024 Posts: 22453 Rating: (3030) |
Hello, i have download it from this locationat 11:29. All zip's are ok. Can it be a problem with you internet Connection? Regards Christoph |
9/23/2013 12:07 PM | |
Joined: 9/23/2013 Last visit: 8/5/2022 Posts: 4 Rating: (0) |
The fail screen |
9/23/2013 1:54 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello mijanmijan Plcheck the Size of the Zip File downloaded. Does it match the Size on the Download Page ? If the Size is smaller then first you should try the download from another PC / another Browser ( Chrome , Frefox etc ). If still this does not work, please take help from Siemens Support. There could be some problem of Casheing of the files. I had the same problem with another download WinCC Prof V11 SP2 Download Problem This was solved with help and support from C S Moderator. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
9/23/2013 3:10 PM | |
Joined: 5/12/2006 Last visit: 11/18/2024 Posts: 22453 Rating: (3030) |
Hello, for the connection problem you can open a new Thread and we will help you |
Follow us on