Industry Online Support
Technical Forum
8/27/2014 1:35 PM | |
Joined: 9/22/2010 Last visit: 7/25/2024 Posts: 225 Rating: (28) |
Hi, it is not allowed to copy migrated, know-how-protected blocks from the migrated project to another project. You always have to use the migrated project. There are two FAQs about this topic, one for the MODBUSPN block and another for the MODBUSCP block: How do you use the blocks for MODBUS/TCP communication over an Industrial Ethernet CP of S7-300 and S7-400 in STEP 7 Professional (TIA Portal)? How do you use the blocks for MODBUS/TCP communication over the integrated PROFINET interface of the S7-300 and S7-400 CPUs and IM151-8 PN/DP CPU in STEP 7 Professional (TIA Portal)? Regards, Sakura |
8/28/2014 10:23 PM | |
Posts: 133 Rating: (2) |
ok thanks, i'll use it |
Follow us on