3/29/2015 1:22 PM | |
Posts: 2 Rating: (0) |
Hi, I too have a following prob, have u any idea / solution - In one of our ships the Exhaust Gas Treatment Unit EGT Model 3 Drewclean EST utilises a PLC – Siemens TD 100 C, Version 1.0.03 to continuously monitor the exhaust trunk temperature, the ship’s air supply pressure and electrical power. When all are within their operating range, the PLC controls the unit’s operation. When any parameter falls out of the accepted range, the unit switches to a standby mode, pauses all functions and then displays the fault description on the operator interface panel. When all parameters return to acceptable range the unit automatically returns to normal operation. The PLC require a one – time initialisation for the ship’s specific configuration.
However the ship has reported that the unit has stopped working on board and :" NO CPU COMM" error message is being displayed on the TD 100 C
May I request you to kindly guide us, as to what could be the probable cause of this malfunction and what remedial measures can be initiated that is spares/parts which may require repair/replacement..
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/30/2015 5:34:36 PMNew subject after splitting |
|
Follow us on