3/22/2017 1:34 PM | |
Joined: 4/23/2010 Last visit: 11/14/2024 Posts: 8092 Rating: (878) |
Sucessor product for 6SC6506-4AA02 is simodrive 611 (please refer this link) , which is also discontinued product now. But with the motor detail namplate you can select from the latest Sinamics series. Or else, provide application, motor & old drive name plate details so that forum memebr may help you. |
3/26/2017 12:27 PM | |
Joined: 4/23/2010 Last visit: 11/14/2024 Posts: 8092 Rating: (878) |
Hello, Is it only spindle axis i.e. speed control or rotary positioning axis also? |
3/27/2017 2:55 PM | |
Joined: 9/10/2007 Last visit: 8/13/2024 Posts: 78 Rating: (3) |
Hai Only speed control... No need of Positioning Chinna |
Follow us on