10/17/2017 11:53 PM | |
Joined: 7/2/2016 Last visit: 5/7/2024 Posts: 115 Rating: (29) |
Hello andrewdaw1978, please check attached wiring diagram example. |
hope this help, if it was helpful please rate the post! |
|
10/18/2017 7:23 AM | |
Posts: 200 Rating: (6) |
Hi Thanks for getting back to us please see attached my out put from my controller. not sure if it will work AttachmentDoc1.pdf (284 Downloads) |
10/18/2017 8:12 AM | |
Posts: 200 Rating: (6) |
Hi My controller is the omega CN245 which is currently fitted in the panel which has a PT100 connected to it I have attached the manual on page 13 it the 0-10v out put https://www.omega.co.uk/pptst/CN245.html AttachmentM5304.zip (438 Downloads) |
10/18/2017 9:36 AM | |
Posts: 200 Rating: (6) |
This is great i have something as always thanks for the help. Would it be OK for you to have a look the simple program and i mean simple as the out put seems to flicker. All i am after is to have the temp controller turn on at 20 and off at 5 which i have working fine its how it works with the 0-10v that i am not sure i have set up correctly AttachmentCircuit Diagram1.zip (248 Downloads) |
This contribution was helpful to1 thankful Users |
10/18/2017 9:56 AM | |
Joined: 12/18/2014 Last visit: 5/21/2024 Posts: 33080 Rating: (4085)
|
What ist the temp range of the 0-10V signal? 0 - 100 °C? Or other? |
10/18/2017 10:02 AM | |
Posts: 200 Rating: (6) |
switch on at 20 °C switch off at 5 °C |
10/18/2017 10:09 AM | |
Posts: 200 Rating: (6) |
0 - 10V correspond to 0 -100 ° C |
10/18/2017 10:22 AM | |
Joined: 12/18/2014 Last visit: 5/21/2024 Posts: 33080 Rating: (4085)
|
In attachment the diagramm with the settings
AttachmentCircuit Diagram1.zip (204 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on