8/10/2020 1:47 PM | |
Joined: 1/10/2020 Last visit: 1/27/2023 Posts: 2 Rating: (0) |
Now i’m working on a Project with the energy manager pro v7.2. i have two computers also, i installed EnMPRO server on the fisrt work station ( PC 1 ) and the EnMPRO Acquisition component and the wincc v7.5 are installed on the second one ( PC2).the acquisition component will serve to collecte the data from the wincc and send the to the main server so they have to be connected to communicate. the PC1 have the foulloing configuration : Dell : optiplex 5060 / windows 10 ( 64 bit) / name of the pc : ENMS / language : french / Excel 2016 / EnMPRO SERVER ( english ) the PC2 have the foulloing configuration : Dell : optiplex 3040 / windows 10 ( 64bit ) / name of the pc : ENMA1 / language : french / Excel 2016 / EnMPRO acquisition module (english) + WinCC v 7.5 the problem is when i try to connect the EnMPRO acquisition component with the EnMPRO server to communicate them i got this : can not connect to master protal (The error information please see the attachment picture1 ) even i login with the adress on the acquisition manual : http://ENMA1/EnMRPOAcquisition/login.aspx the server is still not reachble (The error information please see the attachment picture 2 ) How can i do ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/11/2020 08:03:58New subject after splitting |
|
11/1/2020 9:07 PM | |
Joined: 1/27/2009 Last visit: 5/2/2024 Posts: 42 Rating: (1) |
Did you solve the problem? i have the same problem. Best Regards, Ciwa |
12/14/2020 6:41 AM | |
Posts: 1 Rating: (0) |
IIS? |