5/15/2020 5:08 AM | |
Posts: 17 Rating: (0) |
Dear all, hello. My system is SIMATIC 300 station with CPU 314 IFM 6ES7-314-5AE03-0AB0 . I can not adjust AI4/AO1 integrated CPU (analog_entry_built-in CPU ) I use Simatic Manager Step7 V5.5_SP4_ HF11 download from www.support.industry.siemens.com But utility HW Config does not show AI4/AO1 integrated. If ( in HW Config ) instead of CPU 314 IFM 6ES7-314-5AE03-0AB0 to place on rail CPU 313 C 6ES7-313-5BF03-0AB0 , all OK! I have real only CPU 314 IFM. Please help me in order solving this problem. Prints screen my PC; |
5/15/2020 11:42 AM | |
Joined: 9/27/2006 Last visit: 5/6/2024 Posts: 12257 Rating: (2666)
|
Hello evgeny; This manual shows the wiring diagram for a CPU 314IFM: https://cache.industry.siemens.com/dl/files/591/8860591/att_105766/v1/HB_CPU312IFM_bis_318-2DP_e.pdf See the screenshot below. Hope this helps, |
This contribution was helpful to1 thankful Users |
7/18/2020 4:19 AM | |
Posts: 17 Rating: (0) |
Unfortunately, advices did not help. |
7/22/2020 6:01 AM | |
Posts: 17 Rating: (0) |
I did upload project from CPU , the built-in inputs are not visible. |
7/22/2020 6:03 AM | |
Joined: 12/18/2014 Last visit: 5/7/2024 Posts: 32987 Rating: (4076) |
Have you read the post above yours? |
7/22/2020 7:22 AM | |
Posts: 17 Rating: (0) |
Are you saying that ranges can't be changed? So there is an error in the manual? |
7/22/2020 7:25 PM | |
Joined: 3/28/2015 Last visit: 5/4/2024 Posts: 721 Rating: (213) |
Hello,
Perhaps the following topic might help: How should you connect unused channels of analog input blocks? |
Eng.Mohamed Ibrahim |
|
Follow us on