8/15/2018 3:31 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
Hello! I have new IPC 427E with Windows 10 I installed the Software Controller 1507S F on this IPC. After start CPU virtual screen shows "Connecting...." and after that "Wrong boot option" And I can't load project into CPU. What I do wrong? ------------------------------------------------------------------------------------------ |
Last edited by: pavlan1 at: 8/16/2018 9:39:28 AMLast edited by: Jen_Moderator at: 8/16/2018 10:30:51 AMNew subject after splitting |
|
8/16/2018 11:23 AM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
When I try to reinstall (repair CPU) on the finish It give 2 Error. Log here But first install it install normally AttachmentSIA_CPU_1507SF@18-08-16_11-33-19_summary.txt (744 Downloads) |
8/16/2018 12:37 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
A want to add new information I installed WinCC Runtime Advenced V15 before CPU 1057S F V2.5 |
8/16/2018 1:09 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
When I choose legacy Hard Drive and press Enter I get No bootable device -- insert boot disk and press any key |
8/16/2018 1:25 PM | |
Joined: 5/12/2006 Last visit: 6/7/2024 Posts: 22256 Rating: (2987) |
and is you select efi and press esc after that? |
8/16/2018 1:36 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
then Windows have been loading normally Why ESC? I choose and press Enter. ESC after that not needed |
8/16/2018 3:42 PM | |
Joined: 11/9/2017 Last visit: 6/2/2023 Posts: 44 Rating: (0) |
In Bios are many menu for example [snip] If I choose Boot from file I can find from explorer boot folder and press .efi file [snip] Further is showed this screen [snip] If I press C then is loaded [snip] If Enter then [snip] Further I can't do something more AttachmentImages.zip (665 Downloads) |
Last edited by: Jen_Moderator at: 8/17/2018 8:24:33 AMAdded files as an attachment. |
|
Follow us on