5/31/2024 12:23 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166)
|
Hello, Perhaps the following link might help: No connection to PLC after WinCC Panel Images V17 Update 6 Best regards, Wizard |
6/14/2024 8:41 AM | |
Joined: 8/3/2009 Last visit: 7/17/2024 Posts: 13308 Rating: (1686)
|
Hello AutoGen_5524233 The error code means that there are files missing to transfer the Panel. I would recommend using the Image Installer from this FAQ: https://support.industry.siemens.com/cs/de/en/view/109825750 then install the files for V19 and in this step all the needes Files (additionaly to the single image File)should be present afterwards Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on