7/5/2024 4:26 PM | |
Joined: 5/9/2011 Last visit: 7/12/2024 Posts: 71 Rating: (5) |
Good day All, I am not very experienced in SCL and am trying to create a loop to add values in an array as per the attached. The loop seems to be adding ok but the problem is it does not stop just adding the 15 values for the array. It continues adding infinitely. I need it to only add the values for the array during each cycle and give me the result. At the moment it is not stopping and adding each result to the next result. I hope this makes sense. AttachmentSCL Loop Array addition.pdf (12 Downloads) |
Follow us on