7/21/2024 10:40 AM | |
Joined: 4/28/2015 Last visit: 7/25/2024 Posts: 14 Rating: (0) |
Hi,, I am asking this question again here in this new topic since I could not find solution to my problem. We have a project using CPU315F-2PN/DP and while trying to upload the full project (Software and hardware) I faced the error (The online module 6ES7 315-2FJ14-0AB0 V3.2 does not support uploading to PG). I even tried some of the information provided in this forum: - Tried to add unspecified CPU. - I tried to check the TIA version under Online & Diagnostics / General Tab but I could not find description for TIA version and instead I found Firmware expansion. see attached photo - I also tried to install TIA V16 as one suggested that this option is not available in versions below V16 but this did not help. Thanks,, Attachmenttia upload error.zip (21 Downloads) |
7/24/2024 7:19 AM | |
Joined: 8/6/2018 Last visit: 8/16/2024 Posts: 260 Rating: (40) |
Hello, Are you sure that the PLC is still programmed with TIA PORTAL? Maybe it was programmed with step 7 Thanks you |
Follow us on