8/25/2024 9:47 AM | |
Joined: 11/21/2020 Last visit: 10/17/2024 Posts: 175 Rating: (0) |
Hi, Can you explain how to manage and generate MC-power, jog, velocity, halt, absolute & relative movements errors in PLCSim/reality, if it is possible to test them virtually at all (I'm using 1215C plc and stepper drive CLT57T v4.1)? Which of these errors are critical/reasonable to manage? If one is using this type of drive how it is possible to get any feedback from drive/stepper at all, having in mind that everything work in TIA, but it doesn't mean that drive and motor are present and running? In attachment is tia v19 program with unfinished alarm management section. Thanks AttachmentStepper control.zip (211 Downloads) |
Last edited by: milos23 at: 08/25/2024 09:49:02Last edited by: milos23 at: 08/25/2024 09:50:07 |
|
Follow us on