9/25/2024 2:09 PM | |
Joined: 5/6/2022 Last visit: 10/18/2024 Posts: 470 Rating: (94) |
Hi GeoffN, In this case I think there are two options: 1. If your process allows it (although it seems not), you can remove the OB 121. The CPU then goes to STOP when the error occurs and you can determine in the BSTACK the point in the program where the error occurred. 2. Otherwise, you must search your program for the points where a BCD conversion takes place. There you must check whether the corresponding instructions always receive a number in the correct format.
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
9/26/2024 4:54 AM | |
Joined: 10/7/2005 Last visit: 10/20/2024 Posts: 3024 Rating: (1054) |
In case your program is rather big, you can make searching through it for any and all BCD conversions a bit easier by the doing the following:
|
Cheers |
|
Follow us on