Industry Online Support
Technical Forum
12/4/2009 7:21 PM | |
Posts: 4 Rating: (0) |
I want to add distributed rack to the main CPU (1214C) without using anther CPU but i do not know how can i do that ? |
12/5/2009 12:00 AM | |
Joined: 10/7/2005 Last visit: 9/27/2024 Posts: 3023 Rating: (1054) |
Hello mohamed ibrahim S7-1200's do (currently) NOT support the use of Profibus or Profinet based distributed I/O's. The release of a Profibus DP Master comms module as well as adding Profinet I/O controller functionality to the onboard Ethernet port is however meant to take place towards the end of 2010. I hope this helps |
Cheers |
|
12/5/2009 7:17 PM | |
Posts: 4 Rating: (0) |
thank you |
Follow us on