Industry Online Support
Technical Forum
7/11/2010 10:13 AM | |
Posts: 311 Rating: (3) |
Hello, Can I use this power supply (http://www.meanwelldirect.co.uk/product/DR-120-24/DR-120-24/default.htm) to drive the PLC S7-1200 (CPU 1212C DC/DC/DC). The max start-up current for the PLC is 12 A, and I can not se from the power supply sheet if it manage to drive the PLC at start-up ? Thanks Olof |
7/14/2010 5:46 PM | |
Joined: 5/24/2009 Last visit: 3/27/2024 Posts: 90 Rating: (3) |
So the answer is yes. The shown power supply rates up to 5Amps at 24V. The standard Siemens one is only 2.5Amps... |
Follow us on