1/19/2012 12:20 PM | |
Joined: 9/23/2005 Last visit: 9/25/2024 Posts: 4347 Rating: (1446)
|
Hi, Did you tried to use that? http://support.automation.siemens.com/BR/view/en/56078300 |
Denilson Pegaia |
|
1/19/2012 3:48 PM | |
Posts: 6 Rating: (0) |
Dear Pegia, I have tried with WinCC Tag Converter, to convert the ".CSV" file got from WinCC Flexible Advanced. But, the Tag Converter itself saying that, 0 tags were converted. Still, we got one ".xlsx" file after the conversion operation. Then, I tried to import the same ".xlsx" file into TIA's HMI Tags part.But, I got error message from TIA. Note:- I have attached all the file snap shots during conversion for your reference. Software Used Details: WinCC Flexible is 2008 SP2 Udate 1 TIAVersion V11 SP1 Update 2 Thank You, With regards, Sunil Nath.S
AttachmentFor Pegaia.zip (790 Downloads) |
1/20/2012 12:07 PM | |
Posts: 6 Rating: (0) |
Dear Pegaia, I have clearly mentioned that, while converting the ".CSV" file itself, the WinCC Tag Converter was giving report like, "0-Zero" Tags were converted. Even though, the Tag Converter making one ".XLSX" file with zero tags. Note:- I have attached the ".CSV" file & ".xlsx" file (Got from WinCC Tag Converter). Please try to convert the ".CSV" file with the WinCC Tag Converter and guide me to import it into TIA. Please guide me, If I am wrong in any step. Steps I followed:- 1. I exported the Tags list from WinCC Flexible Advanced. 2. I got one ".CSV" file. 3. Then, I convert the same ".CSV" file to ".xlsx" file with the help of WinCC Tag Converter. 4. I got error reort from WinCC Tag Converter like "0- Tags were converted". 5. But, At the output path location, I found one ".xlsx" file which is created by the converter. 6. I tried to import the ".xlsx" file into TIA and got error message like "No Tags Found".
AttachmentFor Pegaia.zip (739 Downloads) |
Follow us on