Industry Online Support
Technical Forum
4/17/2012 6:03 PM | |
Posts: 19 Rating: (3) |
Hello MKS02, You can have a lookat thisFAQ "With what is SIMATIC WinCC V11 compatible" http://support.automation.siemens.com/WW/view/en/51694087 I suppose the fastest way is to openthe PDF document "WinCC V11 Compatibility List" at the bottom. Best regards |
4/17/2012 7:43 PM | |
Joined: 8/31/2010 Last visit: 9/27/2024 Posts: 1521 Rating: (227) |
Hello el-mare, It seems like MKS02 is asking about integrating a STEP 7 v5.5 project along with WinCC v11. Hello MKS02, Is my understanding right? If so, then this integration of STEP 7 v5.5 project and WinCC v11 is not possible. Whereas if you have a project in STEP 7 v11, then integrating with WinCC v11 is no Big Deal. (also migrating a STEP 7 v5.5 project from STEP 7 v11 is more simple) |
Like it? Rate it! |
|
4/18/2012 10:53 AM | |
Posts: 24 Rating: (0) |
Ah ok. Step 7 V11 it will be thanks |
Follow us on