11/19/2018 3:44 PM | |
Joined: 4/24/2006 Last visit: 8/16/2024 Posts: 8717 Rating:
|
Hello, When you want to add something to the project or you want to change it. You need the original project file. (It is not possible to de-compile the backup of the project Here a link with more information about the cable you can use: Which connector cables are available for connecting to SIMATIC Panels? Best regards, Wizard |
Follow us on