2/1/2024 10:20 AM | |
Joined: 3/30/2020 Last visit: 9/26/2024 Posts: 4796 Rating: (984)
|
Feeding the output pulse back into an input is viable. But it is recommended that you use a high speed counter (HSC). Also make sure that the input is set to the correct filter time. Ensure that the output voltage is at the voltage that the input expect. A handmeter would measure half of the voltage. 24V should measure 12V for a 50% pulse width pulse train. Too much of a degrading of the voltage may also be a problem. Best to not have the stepper motor directly connected to the PLC.
For complete information the following manual is helpful: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on