3/18/2024 3:56 PM | |
Joined: 5/6/2022 Last visit: 9/27/2024 Posts: 455 Rating: (90) |
In the OP270 you have the object that you indicate, the Alarm Indicator, which appears when there are alarms activated and tells you how many. This object I am referring to: "SIMATIC HMI HMI Device TP 177A, TP 177B, OP 177B (WinCC flexible): Displaying Alarms" It can only be inserted into a template. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on