5/25/2007 1:04 PM | |
Posts: 2 Rating:
|
I'm new at the forum. I'mTurkish so excuse me for my english. I have Simodrive611U with 1FK7 servo motor. I must control this system with S7-300 via profibus. But i have no idea what can i do... |
Last edited by: sahcihan at: 25.05.2007 13:05 |
|
5/25/2007 4:52 PM | |
Posts: 328 Rating:
|
Dear Sir The connection and operation of your 1FK motor to S7 via 611U on profibus is not a simple task. I would suggest havng a look at the following link to start with. The give our Turkish Office a call, Im sure they can help you further. You will need to parameterise the 611U using Simocom U software.Then setup coms to the PLC, you will need a profibus module for the 611U https://www.automation.siemens.com/doconweb/content.asp?item=23031&cd=sinumerik_0107_e&scope=all best regards SteveJ |
5/31/2007 10:20 AM | |
Posts: 2 Rating:
|
I did everything about SimoDrive. I must now Control Telegramms. The all of SimoCom paremeters is ok. what can i do about control telegramms. Do i need some software? (for example Drive-ES) |
6/4/2007 5:57 PM | |
Posts: 271 Rating:
|
Greetings: Since you already have SimoCom U software, the easiest way to control Simodrive 611U by Simatic S7-300 is by using the Simodrive 611U Toolbox. The toolbox can be downloaded from the same place you obtained the SimoCom U software or it should be located on the CD you received. There is a special function block (FB83) written by Siemens and there is documentation available in English and German for this. You will need to select PPO type 5 which is described in the 611U Function Description Manual. First configure your hardware in STEP 7 and then call FB83. There are seveal parameters that need to be set in FB83 to get it to work for you. It's not that difficult. Hope this helps... |
This contribution was helpful to
1 thankful Users |
Follow us on