(0)| 6/5/2006 2:53 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Izzy, To find this error you may try it first in testmode on the FM453. Have you give all the data thats necessary in the User Data block? Do you trigger the data on the right time, so have you first set the FM in the MDI-mode before transfer the MDI-Block itself, you can check it back with the check-back signals. You have to do it one by one when you want that the FM do something for you! [:P] So try it first in the test-mode and see in what order you have to do it and what are the checkback-signals. After that you have to built that in the software, because the 400 CPU is faster then you are in the test-mode, the checkback-signals have to be looked at to do the next step. See the little example i have used with the FM453 for several times: AttachmentMDI.zip (1137 Downloads) |
Last edited by: Late at: 6/5/2006 3:01 PMI hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on