11/17/2022 7:46 AM | |
Joined: 11/27/2020 Last visit: 2/1/2023 Posts: 14 Rating: (0) |
Hi, i am also trying to run TIA-Portal on a macbook pro m1 with Parallels 18.0 and Win 11 22H2. I am using Macos Ventura and can install TIA-Portal V17 with WinCC Unified. I have got some questions: - Is it only possible to Install WIncc Unified or also WinCC Prof? My Setup is always crashing. [snip] Thanks a lot. BR Stefan ------------------------------------------------------------------------------------------ |
Last edited by: Stefan-83 at: 11/17/2022 11:22:19Last edited by: Jen_Moderator at: 11/17/2022 11:56:59New subject after splitting. Division of questions into separate topics. |
|
11/17/2022 11:58 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
you can also install winccprof but not on the same vm |
11/18/2022 8:25 AM | |
Joined: 11/27/2020 Last visit: 2/1/2023 Posts: 14 Rating: (0) |
If i try to install WinCC Prof it is always crashing at the setup on my configuration. BR Stefan |
11/18/2022 8:37 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
attach the crash dump |
11/18/2022 11:33 AM | |
Joined: 11/27/2020 Last visit: 2/1/2023 Posts: 14 Rating: (0) |
i will try but first of all is it possible to run the Automation license server? BR Stefan |
11/18/2022 11:42 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
yes is possible |
11/20/2022 11:00 AM | |
Joined: 11/27/2020 Last visit: 2/1/2023 Posts: 14 Rating: (0) |
okay and how? with configuration i should use? |
11/25/2022 7:13 AM | |
Joined: 11/27/2020 Last visit: 2/1/2023 Posts: 14 Rating: (0) |
Hi, anything more you can tell me? BR Stefan |
11/29/2022 10:29 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735) |
Hello Stefan If you only want to inistll the ALM without fram Setup of TIA Portal then you can download the Installation here: https://support.industry.siemens.com/cs/de/en/view/114358 Bye Murof |
If this Information really helps, you could use the Rate function |
|
12/2/2022 9:21 AM | |
Joined: 11/27/2020 Last visit: 2/1/2023 Posts: 14 Rating: (0) |
Hi, if i install ALM first then everything works fine. Problem solved. BR Stefan |
Follow us on