1/8/2023 5:30 PM | |
Joined: 11/27/2013 Last visit: 1/27/2024 Posts: 5 Rating: (0) |
I have the exact same issue my connections in the HMI's tag table are all red. I had to replace the PLC to a newer CPU. did the change & PLC runs 100%. The HMI tags will not compile: Error; "The PLC referenced by the PLC tag cannot be reached thru the configured connection. " HMI Tags > Connections - the connection seems correct, I tried synchronizing the tags (with all the options below it, result states: Syncronization with PLC tags completed, but the connection stays red. The answer above of linking the tags points to an incorrect post. How do I link the tags? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/09/2023 12:02:34New subject after splitting |
|
Follow us on