1/10/2023 3:27 PM | |
Joined: 8/29/2017 Last visit: 11/9/2023 Posts: 10 Rating: (1) |
Dear colleagues I´m looking for a device thats comply with these requeriments: - Processor capable of works with sample rate between 300MHz a 30KHz We test it on a standar raspberry ARM y x86. - Memory 350KBytes RAM, 250KBytes of minimum storage - Communications, modbus tcp.. I´m looking for technnical data but... no suscessfull. Not sure if we need an indusrtial PC or a PLC... Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/11/2023 09:16:50New subject after splitting |
|
1/11/2023 2:47 PM | |
Joined: 2/17/2020 Last visit: 5/13/2024 Posts: 1001 Rating: (171) |
Hi Solar-Laso, I recommend using the TIA Selection Tool as a first approach. And if that weren't enough... it might be convenient for you to discuss this with a sales contact because surely there are many parameters and needs of your specific application to take into account. |
A rating will be well appreciated. |
|
Follow us on