1/24/2023 9:55 AM | |
Joined: 6/18/2021 Last visit: 9/16/2024 Posts: 27 Rating: (0) |
Dear sir, I'm using logo PLC with analog module AM2 for my Air-conditioning application, with following pressure transducer is connected to read R22 refrigerant actual presure From this I can read read R22 refrigerant actual presure but simultaneously I want to read it's pressure corresponding temperature from this presure temperature chart Soo plz kindly help me with eg how to program for this Thanks regards Paigambar A Momin AttachmentR22-PT-Chart (1).pdf (759 Downloads) |
1/24/2023 10:10 AM | |
Joined: 6/18/2021 Last visit: 9/16/2024 Posts: 27 Rating: (0) |
Dear sir, Plz find attached sensor detail for Power supply... 24 VDC controling signal... 0 TO 10 VDC PRESURE... -1bar to 29 bar or -14.5 psi to 420.6 psi Thanks regards Paigambar A Momin AttachmentA6V10448424_Pressure Sensors for refrigerants incl. ammonia QB_en.pdf (812 Downloads) |
Last edited by: Momin paigambar at: 01/24/2023 10:17:46Last edited by: Jen_Moderator at: 01/24/2023 12:12:55Post shortened. |
|
Follow us on