1/28/2023 10:55 AM | |
Joined: 9/10/2021 Last visit: 1/31/2024 Posts: 5 Rating: (0) |
Hello, thank you for the quick suggestions and help. I'm sorry but I do not understand how to do this: "VM mapping of the actual counter value, which then can be changed directly over Modbus as 32 bit unsigned integer.". Could you please elaborate it a little more? I would prefer this VM mapping approach and if not possible, then anything, where from modbus single modbus protocol transaction could set the speed i.e. writing multiple (programmatic) coils at once The lsc diagram of draft version is now attached Attachmentlocal_and_remote_draft.zip (642 Downloads) |
1/28/2023 12:36 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33809 Rating: (4200)
|
|
1/28/2023 12:44 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33809 Rating: (4200)
|
See attached LSC.
Attachmentlocal_and_remote_draft_V2.zip (530 Downloads) |
Follow us on