2/5/2023 8:29 AM | |
Joined: 3/11/2019 Last visit: 4/26/2024 Posts: 1378 Rating: (244) |
Hi Alex, as far is I know, the SP306 can not offically be used is PG M3, at least there is an offical post in german forum, link below (maybe you can use translator). Nevertheless, there is stated tat only batterys SP304 and SP305 (both discontinued) could be used with PG M3. Maybe it is worth creating an support request in this regards to receive official information. SIMATIC Field PG Ersatz-Akkuregards sancruz |
Feedback appreciated, please rate |
|
Follow us on