2/4/2023 9:15 PM | |
Joined: 3/5/2017 Last visit: 9/23/2024 Posts: 776 Rating: (127)
|
Still no need for any triggers. Use click event of a button to set bit and reset after on PLC. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/07/2023 04:57:09New subject after splitting. Quote inserted. - Trying is the first step towards failure. |
|
2/5/2023 5:37 PM | |
Joined: 3/30/2020 Last visit: 9/24/2024 Posts: 4781 Rating: (982) |
Did I miss something? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
2/6/2023 7:07 AM | |
Joined: 3/5/2017 Last visit: 9/23/2024 Posts: 776 Rating: (127)
|
I probably missed something. I thought that @rfriedman is going to use push buttons on HMI and still positive edge triggers on PLC. I base this of comments about operator feel, so most likely a button on HMI. So I only commented that there is no need for triggers on PLC, whether the action is on positive - or negative edge.
|
- Trying is the first step towards failure. |
|
2/6/2023 7:56 AM | |
Joined: 3/30/2020 Last visit: 9/24/2024 Posts: 4781 Rating: (982) |
Your recommendation for not using a positive/negative edge when using a button on an HMI is a sound one. It is also a good suggestion to use the Set Bit function and have the PLC reset the bit tag. Though I am not sure why you suggest the "click event" of the HMI button, unless that was not meant literally. Or perhaps it is a suggestion to suit a mouse operated WinCC session. I use the "release key" event on the Basic Panels. My point?.. For my own education: Which situation is "click event" best used for? Is this event on the release of the mouse button / touch? |
Last edited by: qwazee at: 02/06/2023 07:57:01Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on