2/6/2023 12:40 PM | |
Joined: 3/4/2020 Last visit: 4/2/2024 Posts: 29 Rating: (0) |
I think I'm facing the same problem with a MCU1720 (PLC 1500 integrated) with a S210 PN drive. SINUMERIK ONE Commissioning shows just "2000048 < no text available>" , but our customized interface shows the correct message "2000048 Maintenance Demanded : Multi-Interface Mismatch - Name of Station of Interface is Not Unambiguous". The diagnostic of this drive in TIA Portal v16 is not showing any Active alarm, but PLC shows a warning on that Drive: "Maintenance demanded, Error in Lower-Level component" There are 6 drives hanging from port X150_1, so all IRT devices in line and no switch present. No other device is giving warnings or alarms and all of them had the same setup procedure, included the paired drive of the slave axis of the gantry (the drive that gives the alarm is the master of the gantry). The machine works with no problem, but it just shows the alarm on the HMI of the customer and it's annoying. Any idea? ------------------------------------------------------------------------------------------ |
Last edited by: Boskyman at: 02/06/2023 12:43:44Last edited by: Boskyman at: 02/06/2023 12:48:36Last edited by: Boskyman at: 02/06/2023 12:52:04Last edited by: Jen_Moderator at: 02/07/2023 08:57:25New subject after splitting Living between Spindles, Waterjet heads and Lasers... |
|
Follow us on